AXIS#.VL.LIMITN

Description

AXIS#.VL.LIMITN sets the velocity command negative limit.

If the input to the velocity loop is lower than AXIS#.VL.LIMITN, then the actual velocity command AXIS#.VL.CMD is limited by the value of AXIS#.VL.LIMITN.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s

See Velocity Units for details.

Range

Depends on units. See Velocity Range for details.

Default Value

15000 RPM

Depends on units. See Velocity Units for details.

Data Type

Float

See Also

AXIS#.VL.LIMITP, AXIS#.VL.CMD
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
AXIS1.VL.LIMITN

5011h

07h

Signed32

Velocity

-

Read/Write

No

AXIS2.VL.LIMITN

5111h

07h

Signed32

Velocity

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.VL.LIMITN

6031

178F

Signed32

Read/Write

Velocity

AXIS2.VL.LIMITN

71567

1178

Signed32

Read/Write

Velocity

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.VL.LIMITN

6031

Float

Read/Write

Velocity